Multiple Components

When you select a single component on the map, the Component Information pane automatically displays the attributes for that component.

When you select multiple components on the map, the pane organizes the components by component type and displays their Facility IDs (they are also sorted alphanumerically by Facility ID).

From that point, you can:

  • Double-click a component’s Facility ID to view its attributes.

  • To return to the full list, in the upper, right-hand corner of the Component Information pane, click the View All button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?