Hide Component

To reduce clutter on the map, perhaps you want to hide nearby components that are not directly involved in your design. You can accomplish this using the Hide tool.

IMPORTANT:
  • The Hide tool hides both the component and its label.

  • You can hide components you sketched, and you can hide existing components you did not sketch.

  • You can use the Hide tool in the Design tab or the Layout tab.

    • If you Hide components on the Design tab, they are also hidden on the Layout tab.

    • However, if you Hide components on the Layout tab, they are still visible on the Design tab.

To hide a component, right-click an individual component and choose Hide. Or, use the Select by Rectangle tool to select many components. Then, right-click and choose Hide

TIP: You can Undo the Hide tool.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?