Hotkeys

Hotkeys are keyboard shortcuts. They are invaluable time savers. Most often, when you have the tool active in the design, it displays its hotkey for future reference.


Map

Map

CU search

Ctrl+F

Save Design

Ctrl+S

Redo

Ctrl+Y

Undo

Ctrl+Z

Zoom In

Ctrl++

Zoom Out

Ctrl+-

Go Back Extent

Alt+LeftArrow

Go Forward Extent

Alt+RightArrow

Deletes Selected Component, CU, or Map Notation

Delete

Cycle through Design Styles

Ctrl+Shift+S

Design Tab

Design Tab

Select

Alt+S

Select by Rectangle

Alt+R

Place Transformer

Alt+X

Place Conductor

Alt+C

Place Conduit

Alt+O

Place Pole

Alt+E

Place Span Guy

Alt+J

Place Surface Structure

Alt+Z

Place Fuse

Alt+F

Place Recloser

Alt+B

Place Switch

Alt+I

Place Service Drop

Alt+V

Place Electric Network Component

Alt+G

Place Generic Line Component

Alt+L

Place Load Break Switch

Alt+U

Place Sectionalizer

Alt+Shift+T

Place Work Location

Alt+W

Replace

Alt+Shift+R

Trace

Alt+T

Measure

Alt+M

Place Cut Point

Alt+Y

Address Search

Alt+A

Update Catalog

Ctrl+Alt+U

If on the Layout Tab, switch to Design Tab

D

Run Auto-Assign Work Location

Alt+K

Copy current XY location to clipboard

Ctrl+L

Toggle display between projected XY and latitude/longitude

Ctrl+Alt+L

Cycle Through Label Styles when Using the Move Label Tool

A to cycle forward through styles

Z to cycle backward through styles

Design Tab Tool Modifiers

Design Tab Tool Modifiers

Disable Snapping

Spacebar

Snap to line features, but not point features while the hotkey is held

Press and hold e

Lock in Preferred Transformer when using Place Service Drop

Ctrl

NOTE: The Place Service Drop tool automatically snaps the service line to the nearest transformer. To temporarily override this functionality (in order to “lock in” a preferred transformer that might not be the closest in proximity), first allow the tool to find and snap to your preferred transformer. Then, hold Ctrl while moving the service meter into position. This keeps you snapped to the preferred transformer, even if other transformers are nearby. If your service line is straight (no bends), double-click to finish the sketch. If your service line has bends in it, each click adds a bend. After you add your first bend, you can release Ctrl. Double-click to finish the sketch. For more information, read the topic Place Service Drops.

Finish Linear Sketch

Enter

Finish Linear Sketch

Double Click

Cancel Selected Tool/Action

Esc

Pan map when in Remove Brush tool mode

Ctrl+Drag

Layout Tab Label Placement

TIP: See the topic Label Individual Components to see these hotkeys in action.

Layout Tab Label Placement

Make Label Angle Match the Page Orientation

Press and hold x, then drag with your mouse

Slide Label and Leader Line Along a Linear Component

Press and hold Spacebar, then drag with your mouse

“Unlock” Label Orientation to Set at Any Angle

Press and hold a, then drag with your mouse

Toggle Label on Either Side of a Linear Feature

Tab

Precision Editing Tools

Precision Editing Tools

Line Mode

1

Follow Mode

2

Arc Mode

3

Distance Angle Mode

4

Place Service Drop Tool Modifiers

Place Service Drop Tool Modifiers

Lock to nearest Service Drop tap

Ctrl (or after first click)

Disconnect Service Point from Service Drop

Shift

Place Service Point in Space

Shift+Click

Sketching Templates

Sketching Templates

Rotate Template Counter-Clockwise

<

Rotate Template Clockwise

>

Flip Template Vertically

n

Flip Template Horizontally

m

Lock Template Angle after Rotating (stops nearby lines from overriding your set angle)

Spacebar (press once, do not hold; press once again to unlock)

Enlarge Template (you can enlarge a template to about twice its originally-drawn size)

+

Shrink Template (you can shrink a template to about half its originally-drawn size)

-

Removes

Removes

Accept Removal CU when Green Hover is Up

A

Select a Removal CU when Red Hover is Up

C

Project Pane

Project Pane

Delete Selected Component or CU

Delete

Trace Tool Modifiers

Trace Tool Modifiers

Lock highlighting

L

Lock highlighting

Enter

Unlock highlighting

U

Unlock highlighting

Esc

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?