Stamp Graphics Pane

Stamp Graphics provide non-network graphics and text blocks to add to your Design or Layout. They are typically used to add helpful details and notes about the design area. The graphics and text are not pushed back to the GIS.

The default behavior for stamp graphics is to be placed on top of the network features. Because this may obscure some features, it is possible to set the z-index of individual stamp graphics to place them underneath the network layer. See Setting Stamp Graphics Layer.

Designer XI provides a sample set of graphics and text options. Each company configures graphics to suit its needs, so your graphics are likely different than those seen in the images throughout these help topics.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?