Pole Attachments

The Click Wheel for poles provides a fast way to add attachments including assemblies, risers, and guys.

IMPORTANT: You can add risers and guys to both new and existing poles, but you can add assemblies only to new poles.

  1. Right-click a pole.

  2. Next to +Attachments, click the green arrow to expand to more options.

  3. Click which attachment to add. Again, assemblies are available only for new poles.

  4. The CU Search appears automatically filtered to the chosen attachment type.

  5. Find your desired CU, then double-click it to add to the pole.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?