Layout Tab

The Layout tab is the interface for creating the maps and documentation needed to share your designs with others.

It allows for different map views, labels, and text block configurations to display what you want and where you want it. Administrators can (and should) also create templates to support quick and easy print jobs.

By default, the tab at the top of the interface is “locked” in a position where it is visible at all times. Double-click the tab to enable auto-hide, where the tab collapses while you interact with the map or other panes. To return to the locked position, double-click the tab again.

Keep reading the subtopics in this help chapter to learn more about creating printable design maps.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?