Settings

This tab shows available packages for download and the application information. Packages typically include an offline basemap in TPK format and a replica of the network. They allow for offline design work on the application.

IMPORTANT: A basemap is required for the application to be able to open a design. If you are connected to the internet, then it can stream a basemap. However, if you are planning on doing work while disconnected from the internet, then you must download a package prior to going offline.

The Available subtab displays packages that have been created and made available to you.

Icons indicate the status of the package:

  • Available : The package is ready to download. Click to begin.

  • Downloading : The package is in the process of downloading. Click to cancel the download.

  • Downloaded : The package has successfully downloaded. The package moves to the Downloaded subtab upon refreshing the screen.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?