Add One Unit or Subtract One Unit

  1. In the Project pane, find the Non-Drawn CU where you want to change the quantity.
  2. Hover over the options icon for that Non-Drawn CU, then click either the add or subtract one unit buttons to increment the quantity by 1.

    TIP: If the quantity is already set at 1, clicking the Subtract One Unit does not do anything. If your intent is to remove the unit, click it and press Delete.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?