Other Component

A gas component is a point feature. Not all types of gas features are currently supported in the application. A gas component is a generic feature against which a specific feature CU can be assigned. Eventually, these gas features might be included in the standard Design tab. In the meantime, when you require one of those features not represented on the Design tab, use a gas component instead, specifying the gas device CU required.

Sketching

  • Gas components snap to pipes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?