Navigation Tools
Ease of navigation is just one highlight of Designer XI.
Pan
-
While viewing the map, simply click and drag the mouse to pan. This works even when you have another design tool active and even if you are mid-sketch. There are only a few exceptions to this:
Zoom
-
To zoom, use the scroll wheel on your mouse. Pushing the wheel forward zooms in and pulling the wheel back zooms out.
-
As an alternative, press Ctrl and the plus sign (Ctrl +) to zoom in, and Ctrl and the minus sign (Ctrl -) to zoom out.
-
Further, press Shift, then drag your cursor to create a “zoom to” box. The map zooms to the area you outlined with your box.
Previous/Next Extent
-
The Previous and Next Extent
tools are located in the lower right-hand corner of the application.
Click the Previous Extent tool to move back to a previously-viewed
location on the map. Alternatively, if you have moved back to a location
and want to return, use the Next Extent tool. -
As an alternative, press Alt+Left for the previous extent, and Alt+Right for the next extent.