Arc Mode

Arc Mode allows you to sketch smooth arcs within your design. This mode is most commonly used for underground installations.

While sketching, the application displays the bend radius for the upcoming portion of the line. Keep track of this radius to ensure you are sketching arcs within an acceptable bend range.

GIF showing Arc mode in magenta on a map background.

Your cursor stays in Arc Mode click after click until you either switch to another mode or finish the sketch.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?