Edit Quantity

Do you need to change a Non-Drawn CU quantity by a large amount? Instead of clicking the Add One Unit or Subtract One Unit buttons several times, use the Edit Quantity button to type the desired number.

  1. In the Project pane, find the Non-Drawn CU where you want to Edit Quantity.

  2. Hover over the options icon for that item, then click the Edit Quantity tool.

  3. Type a new quantity, then press Enter.

TIP: Want an even faster way? Click directly on the existing quantity number. This activates the field. Then, type a new quantity and press Enter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?