XY Tool

In the lower, right-hand corner of the application, there is an XY tool.

With a single click of the XY tool , you can toggle the cursor’s longitude/latitude label text on and off.

Toggled On :

Toggled Off :


Change Display Units

Use the Hotkey Ctrl+Alt+L to toggle between projected XY coordinates and latitude/longitude.


Copy Location

Use the Hotkey Ctrl+L to copy the current location to your clipboard.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?