Save in Parallel

IMPORTANT: When you are offline, the app saves locally only.
  1. While saving, you can perform other actions in the map without being locked out.
  2. You can’t leave the app or you receive a warning.

  3. If the design fails to save locally, you are given a notification.

  4. If the design fails to save to the server, you are given a different notification.

  5. If it fails to save locally and to the server, you are prompted to retry the save or to not save at all.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?