Surface Structure

A surface structure is used in underground installations. The types are driven by your CU library, but these often include pads, pedestals, handholes, etc.

Sketching

  • Click in the map to place new surface structures. Each click adds a structure.

  • Surface structures do not snap to other devices or conductors. However, when sketching conductors, the conductors snap to existing structures.

  • Surface structures can also snap to guide points for precision placement.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?