Copy All CU Text

This tool located at the bottom of the Project pane is similar to the Copy WL CU Text tool, except it copies the information from all Work Locations instead of just one.

To Copy All CU Text:

  1. At the bottom of the Project pane, click Copy All CU Text.

  2. Paste as needed, for example, in a Map Note for printing purposes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?