Workflow and Tasks

The Workflow and Task tools are located In the center of the interface.

The names of the states, actions, and Tasks are configurable and vary by customer. The image is just an example.

The availability of Workflow states and certain Tasks depends on the status of your design. If you think a Task or Workflow state should be available but it is grayed out for you, check with your administrator first to see if your design satisfies the requirements of that particular state or Task.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?