Line Mode

Line Mode is the default precision editing tool while sketching conductors, pipes, or any generic line component.

Each click places a vertex (or bend point) along the line. While sketching, the application displays helpful information about your sketch, including total length thus far, current length of the upcoming portion of the line, and current angle. Holding Ctrl during placement automatically snaps to the closest angle of 0, 30, 45, 60, 90, 120, 135, 150, or 180.

Map image showing multiple line segments in magenta.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?