Modify Stamp Graphics
After placing a Stamp Graphic, you can right-click it to access modification tools.
The available modification tools depend on the type of graphic.
-
Copy Element: This creates a duplicate of the graphic. Click to place the duplicate in a desired location.
-
Edit Geometry: For lines, this “re-opens” the graphic sketch. You can click a vertex (or bend) along the line, then drag into a desired position.
-
Edit Text: For text, it re-opens the text editor dialog. There, you can change the text itself or the formatting of the text.
-
Delete: This deletes the selected graphic.
TIP: You can also select the graphic and press the Delete key instead of right-clicking. -
Move: This allows you to move the entire graphic. Click to place in a desired location. When moving a graphic, you can snap to guide points for precision placement.
-
Resize and Rotate: For polygons, this “re-opens” the graphic sketch. You can click and drag a node along the polygon to resize. You can click and hold the Rotate
button to rotate the entire graphic.