Hosted Workflows
The Hosted subtab, or workflow family, is the home of hosted workflows that might include the Session Manager workflow, Designer workflow, Feeder Services workflows, and Markup workflow for Mobile.
Hosted workflows can orchestrate business processes. They deal with movement of work across systems (think: sending information from Mobile to Designer or Editor. These are hosted on shared architecture in Microsoft Azure Cloud. These workflows are capable of things like publishing service bus messages and working with service bus infrastructure. They can be triggered by a scheduled event, or when a specific action happens.
The concept of hosted workflows is different from client-side workflows in that client-side workflows take place on a client machine and affect an individual user’s experience within a specific application. An example of a hosted workflow might be the entire Session Manager workflow whereas an example of a client-side workflow might be Open Session from within Editor.
Available Tools
The functions, tools, and subtabs are largely the same between the Studio and Default Workflow Studio tabs. However, the Studio tab provides a few additional tools on its subtabs. Refer to the Studio topic in the ArcFM Solution Center Implementation Guide to learn about the additional tools.
The following buttons are available on all subtabs in Default Workflow Studio:
Revision history of a workflow is recorded and can be helpful to track changes made to different versions of workflows over time. Refer to the Default Workflow Studio topic to read more about revision history records.
Below is an example of a hosted workflow, the Session Manager workflow.
Workflow Properties
| Property | Definition |
|---|---|
|
Name |
The title of your workflow. |
|
Minimum Client Version |
The minimum version of Editor required to execute this workflow. This field applies to autoupdater workflows on the ArcGIS Server subtab, and workflows on the Editor Client subtab. Drop-down values on the ArcGIS Server subtab begin with 2024 C1. Drop-down values on the Editor Client subtab begin with 2025 C1. We recommend leaving this field blank on all other types of workflows. |
|
Workflow Status |
Published — the workflow is published and represents the latest version of the workflow. Draft — the workflow is in draft form and not published. Retired — the workflow has been replaced by a newer version and this version is retired and no longer published. Example — this is a workflow example that is useful for copying and pasting into a new workflow as a template or starting point. |
|
Workflow Metadata Id |
The unique identifier on each version of a workflow that allows you to call a particular version. |
|
Workflow Ancestral Id |
This identifier designates the starting point of a workflow’s history, after which all versions maintain that Ancestral Id. |
|
Version |
The version number of the workflow. Useful in tracking the evolution of workflows as administrators make changes. |
|
Updated By |
The user name of the last person to modify the workflow. The OOTB workflows provided by Schneider Electric say Updated By Schneider Electric Team, or sometimes say none. |
|
Updated On |
The date the last workflow modifications were made. |
|
Expression Language |
The coding language that is used within the workflow. |