Configure Solution Center

To properly configure Designer XI, most of the configuration must be completed in Solution Center within the Designer plugin.

Go to the myArcFM article ArcFM Solution Center to find out more about the application and to download the installer, if not already installed.

NOTE: Solution Center has its own configuration guide! See ArcFM Solution Center – Implementation Guide for more information.

This section covers all the possible Designer XI configuration within Solution Center; however, not all settings are required to complete your installation of Designer XI.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.