Software Version 2.14.0

Shutter Relay

The Shutter Relay device is a C-Bus relay output unit for controlling motorised blinds, curtains, and window shutters. It also allows natural light to be incorporated into a lighting solution.

Prerequisites:

  • A project must be open in the SpaceLogic C-Bus Commission software. The Shutter Relay device must already be added to a Devices in Project of a network (Adding Shutter Relay is similar to adding any C-Bus device).

  • This section displays the name and type of the Shutter Relay device. The name of the Shutter Relay device can be renamed and also allows the user to configure different operational features for Shutter Relay devices added to each network.

  1. Select a Network from the project.

  2. Click C-Bus Devices of a network.

  3. Select Shutter Relay device from Devices in Project. The selected Shutter Relay device properties are displayed in the PROPERTIES window.

    NOTE: The fields in the device properties can be modified as per the project requirement.
  4. The field information to configure SpaceLogic C-Bus Shutter Relay is explained below:

    Applications

    This section displays the lighting applications supported by the Shutter Relays. Only one lighting application can be defined and then used throughout the configuration of the Shutter Relays.

    • Click . The Add Application pop-up appears.

    • Enter the required details and then click Create. The application is created and listed in the Application 1 drop-down.

    • Click to modify the application name.

    • Make necessary changes and then click Save.

    Channels

    NOTE: RELDB1 will have 1 channel

    Group

    This field allows to program group addresses associated with Shutter Relay channels.

    • You can select group address using drop-down.

    • Click to add group address. The Add Group pop-up appears.

    • Enter the required details and then click OK. The group is created and listed in the Group drop-down.

    • Click to modify group address. The Edit Group pop-up appears.

    • Make necessary changes and then click OK.

    You can also create a new group name which takes the next available address (it’s a fast commissioning option).

    Fail Safe Duration

    Select the time for fail safe duration from the drop-down.

    Change Over Delay

    Select the time for minimum delay permitted between completing an open or close operation and commencing another.

    Level Translation Mode

    If you uncheck the Level Translation Mode check box, a Confirmation pop-up appears.

    Click Yes to disable level translation mode.

    Global

    This section displays the project properties set by the user at the time of creation of the project.

    Area

    This field displays the area address, which is set to unused by default. You can use the Area drop-down to program the unit to be part of a specific area.

    • Click to add group address. The Add Group pop-up appears.

    • Click to modify group address. The Edit Group pop-up appears.

    Unit Options

    Enable C-Bus Clock

    If checked, you can enable the C-Bus clock for the Shutter Relays.

    Enable Burden (Software)

    You can enable/disable the Enable Burden check box only if the unit address is set to 1 and the Enable C-Bus Clock check box is selected.

    Enable Local Toggle

    If checked, you can enable the local toggle for the Shutter Relays.

    Enable C-Bus Priority

    If checked, you can enable the C-Bus priority for the Shutter Relays.

    Learn Mode

    Allow Learn Mode

    Select the Allow Learn Mode check box to enable the Application Learn drop-down.

    Application Learn

    The Application Learn drop-down is enabled only if the Allow Learn Mode check box is selected.

    Unit Has Learned

    This field displays Yes if the unit has been learned and No if the unit has not been learned.

    Unit Identification

    This section display the fields for identification of the unit.

    Unit Type

    This field displays the unit type and unit description of the device.

    Catalog Number

    This field displays the catalog number related to the unit type.

    Firmware Version

    This field displays the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database.

    Part Name

    This field displays the part name which is stored in the unit hardware, which can be modified.

    Unit Address

    This field displays the unit address assigned to the device.

    Serial Number

    This field contains the serial number which exists on the physical network.

    Tag Name

    This field displays the name that you can provide to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only.

    Notes

    This field displays a location to add notes about the unit which is stored in the project database only.

    Status

    The Status section contains information about the C-Bus network related functions located on the unit.

    C-Bus Clock Active

    This field displays whether the C-Bus internal clock is currently enabled on the Shutter Relays on the network.

    C-Bus Voltage (V)

    This field displays the C-Bus voltage of the device.

    Learn Mode Active

    This field displays the status of the learn mode.

    Burden (Software) Active

    This field displays the status of the burden (software).

    Local Toggle Active

    This field displays the status of the local toggle.

    Once Shutter Relay configuration is completed, Save the changes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.