Software Version 2.14.0

Software Update

The software update feature enables the use of the most up-to-date software, minimizing downtime/disruptions when commissioning projects. This ensures smooth and efficient operation. Additionally, it also:

  • Sends automatic notifications about new software updates/versions.

  • Allows you to install the latest updates for the SpaceLogic Commissioning Software (SLCC) application by integrating with the Schneider Electric Software Update (SESU) platform.

  • Prevents user from clicking the incorrect link on the Schneider Electric website.

To install the software update feature:

  1. Double click the Software Update icon. The Schneider Electric Software Update (SESU) application appears.

  2. Click the Settings tab. The Notifications section is displayed.

    NOTE: You can only view the frequency of notifications to be received.
    • For critical Updates: Weekly reminders on available updates and daily notifications on new updates.

    • For normal Updates: Weekly notifications on new updates.

  3. Click the Updates tab. The SESU application displays all the relevant updates. In case, you missed the updates, click Check for Updates.

    NOTE: Click Don't show this Update again, to prevent updates from appearing. For more information on the SpaceLogic C-Bus application, click Get additional information.
  4. To download the new software update, either:

    • Select one or more update and then click Download.

      or,

    • Select the Select/Unselect all checkbox to select all the updates and then click Download. The new update starts to download.

  5. Once the download is completed, the below screen is displayed.

  6. You can either open the directory containing the downloaded file or directly click Install to initiate the installation process. The new updates will be

    installed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.