DALI-2 Gateway
Unit Type
SYS_DAL2 (5502CDGP230)
The table below explains the field information in the property editor required to configure the DALI-2 gateway device.
Applications This section displays the lighting applications supported by the DALI-2 gateway. Up to four lighting applications can be defined and then used throughout the configuration of the DALI-2 gateway for control across C-Bus Main, Line A and Line B. |
||||||
Main |
||||||
Configuration This section has a configuration field to set the operation conditions for C-Bus DALI-2 gateway. |
Broken Device Reporting This section displays the different failure modes. If a failure mode check box is selected, the C-Bus DALI-2 gateway will report that failure mode.
|
|||||
Disable Factory Reset If this check box is selected, the C-Bus DALI-2 gateway will disable the factory reset. |
||||||
Error Reporting This section displays the fields for error reporting. |
Device ID |
This field displays the unit address of the device. When you assign a Device ID, and then if you set the Device ID to Not Assigned, then all properties in both the Error Reporting and Measurement section are reverted to their default settings and disabled (grey out state). Mouse over on the Device ID info icon to view the tooltip message. |
||||
Mode Control Group |
This field allows to add an enable group (0–254). If you assign a group, Restore To Previous field is displayed and Regular Reporting Interval drop-down is enabled. If you uncheck the Restore To Previous check box, Regular Reporting field will be enabled. If you check Restore To Previous check box, Regular Reporting will be disabled. |
|||||
Regular Reporting |
This field configures the regular reporting mode of the DALI-2 gateway into one of the below modes:
All the modes can be set with the regular reporting interval set to No regular reports, which allows live reporting of errors without the regular reports. Mouse over on the Regular Reporting info icon to view the tooltip message. |
|||||
Restore To Previous |
When you click Save with the below conditions:
The Regular Reporting displays the last saved value. Mouse over on the Restore to Previous info icon to view the tooltip message. |
|||||
Regular Report Interval |
This field is used to select the time interval period between the completion of a regular report and beginning of the next report in All Errors, most recent only and All Errors, most recent and most severe modes. By default, the interval is 30 minutes. Regular reporting interval is enabled for Trigger Only mode. |
|||||
Trigger Group |
This field contains a Trigger Group to trigger an error reporting event for any of the three error reporting modes. When a trigger group is created, Resend Action Selector and Acknowledge All Action selector fields are displayed. The Resend Action Selector is set to send all errors and Acknowledge All Action selector is set to acknowledge all errors. |
|||||
Destination Network |
This field contains the destination C-Bus network to which the DALI-2 gateway routes the error messages. This allows the error messages to be sent to a remote C-Bus network for central monitoring if it’s not the local network. Mouse over on the Destination Network info icon to view the tooltip message. |
|||||
Advanced |
C-Bus Voltage Warning Set Threshold |
Mouse over on the C-Bus Voltage Warning Set Threshold info icon to view the tooltip message. |
||||
C-Bus Voltage Warning Clear Threshold |
|
|||||
C-Bus Voltage Critical Set Threshold |
|
|||||
C-Bus Voltage Critical Clear Threshold |
|
|||||
C-Bus Power Supply Warning Set Threshold |
Mouse over on the C-Bus Power Supply Warning Set Threshold info icon to view the tooltip message. |
|||||
C-Bus Power Supply Warning Clear Threshold |
Mouse over on the C-Bus Power Supply Warning Clear Threshold info icon to view the tooltip message. |
|||||
Unit Over Temperature Set Threshold |
This field is a combo box which is by default set to 70 °C. The Unit Over Temperature Set Threshold property increments by 1 °C with a range of 1 °C - 80 °C. Mouse over on the Unit Over Temperature Set Threshold info icon to view the tooltip message. |
|||||
Unit Over Temperature Clear Threshold |
This field is a combo box which is by default set to 65° C. The Unit Over Temperature Clear Threshold property increments by 1° C with a range of 0° C - 79° C. Mouse over on the Unit Over Temperature Clear Threshold info icon to view the tooltip message. |
|||||
Line A Over Temperature Set Threshold |
Mouse over on the Line A Over Temperature Set Threshold info icon to view the tooltip message. |
|||||
Line A Over Temperature Clear Threshold |
Mouse over on the Line A Over Temperature Clear Threshold info icon to view the tooltip message. |
|||||
Line B Over Temperature Set Threshold |
Mouse over on the Line B Over Temperature Set Threshold info icon to view the tooltip message. |
|||||
Line B Over Temperature Clear Threshold |
Mouse over on the Line B Over Temperature Clear Threshold info icon to view the tooltip message. |
|||||
Measurement The DALI-2 Gateway monitors a range of properties such as DALI device lamp running time, line voltage and line current for each DALI line. This information can then be shared on C-Bus using the measurement application. |
Device ID |
This field displays the unit address of the device. When you assign a Device ID, and then if you set the Device ID to Not Assigned, then all properties in both the Error Reporting and Measurement section are reverted to their default settings and disabled (grey out state). Mouse over on the Device ID info icon to view the tooltip message. |
||||
Send Trigger Group |
This field contains a trigger group to request the DALI-2 gateway to send its stored measurement data. Mouse over on the Send Trigger Group info icon to view the tooltip message. |
|||||
Clear Trigger Group |
This field contains a trigger group to clear the stored measurement data in the DALI- 2 gateway. Mouse over on the Clear Trigger Group info icon to view the tooltip message. |
|||||
Regular Broadcast Interval |
Disabled by default. Can set the intervals between 1 min to 4 hours. |
|||||
Regular Broadcast Option |
All |
Enabled by default. |
||||
Lamp Hours |
Selected and disabled by default. |
|||||
DALI MAC Temperature |
Selected and disabled by default. |
|||||
DALI Current |
Selected and disabled by default. |
|||||
DALI Voltage |
Selected and disabled by default. |
|||||
C-Bus Voltage |
Selected and disabled by default. |
|||||
Unit temperature |
Selected and disabled by default. |
|||||
NOTE: Deselecting All check box will enable each of the individual check box options.
|
||||||
Destination Network |
This field contains the destination C-Bus network to which the DALI-2 gateway routes the measurement application messages. Mouse over on the Destination Network info icon to view the tooltip message. |
|||||
Each Device ID assigned has Send Trigger group associated with an Action Selector as described in the below table. |
||||||
Action Selector |
Property |
Units |
Resettable |
Notes |
||
0–63 |
Lamp Running Time (Line A) |
Hours |
Yes |
Indexed By Object ID |
||
64–127 |
Lamp Running Time (Line B) |
Hours |
Yes |
Indexed by Object ID |
||
128 |
Line A DALI Voltage |
Volts |
No |
|||
129 |
Line B DALI Voltage |
Volts |
No |
|||
130 |
Line A DALI Current |
Amperes |
No |
|||
131 |
Line B DALI Current |
Amperes |
No |
|||
132 |
Line A DALI MAC Temperature |
Degrees C |
No |
|||
133 |
Line B DALI MAC Temperature |
Degrees C |
No |
|||
253 |
C-Bus Voltage |
Volts |
No |
|||
254 |
Unit Temperature |
Degrees C |
No |
|||
Logic The DALI-2 Gateway can utilize combinational logic to control lighting behavior for DALI Line broadcast, DALI group or DALI device control. Up to 16 logic groups can be used for a DALI-2 Gateway. |
Logic Groups |
This section allows users to configure a C-Bus group from a lighting application for each of the 16 available logic groups. |
||||
Global This section displays the project properties set by the user at the time of creation of the project. |
C-Bus Clock |
This section allows users to enable or disable the C-Bus clock for the DALI-2 gateway. |
||||
Unit Identification This section displays the fields for identification of the unit. |
Unit Type |
Displays the unit type and unit description of the device. |
||||
Catalogue Number |
Displays the catalog number related to the unit type. |
|||||
Firmware Version |
Displays the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database. |
|||||
Part Name |
Displays the part name which is stored in the unit hardware, which can be modified. |
|||||
Unit Address |
Displays the unit address assigned to the device. |
|||||
Serial Number |
Displays the serial number which exists on the physical network. |
|||||
Tag Name |
Displays the name that user can give to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only. |
|||||
Notes |
A location to add notes about the unit which is stored in the project database only. |
|||||
Status The Status section contains information about the C-Bus network related functions located on the unit. |
Voltage |
Displays the voltage level available to the unit. The voltage level displayed refreshes whenever the Update Status button is clicked. |
||||
C-Bus Clock-Active |
This field indicates whether the C-Bus internal clock is currently enabled on the DALI-2 gateway within the network. |
Line A / Line B |
||||
Line A / Line B name |
This field allows to rename Line A / Line B. |
|||
Warn Before Off Enable Group |
This field allows to create a group to enable application. |
|||
WBO Restore |
This field allows to set the Warn Before Off Restore by selecting the check box. If unchecked, can set the Warn Before Off restore level to Use off level, Use minimum level, or between 1–100%. |
|||
Enable Local Toggle |
This field allows to set the Enable Local Toggle by selecting the check box. |
|||
Enable Commissioning |
This field allows to set the Enable Commissioning by selecting the check box. |
|||
Enable C-Bus Priority |
This field allows to set the Enable C-Bus Priority by selecting the check box. |
|||
Missing Device Threshold |
This field allows to set the missing device range from 1–255. |
|||
Status Update Interval (Secs) |
This field displays the status update interval ranging from 2–255. |
Once configuring of the device is completed. Click Save in the PROPERTIES window to save the changes in the project database.