Software Version 2.14.0

Scan C-Bus Network

Prerequisites: The network must be opened before scanning.

The C-Bus Devices present in the network appears in the Devices on Network section, after the network is opened and scanned. The DALI devices present on the line appears in the Line Devices section, after the DALI line is scanned.

  1. Click to search for the devices in the network.

    NOTE: If network scanning is done without opening the network, internally the network is opened first and then scanning is performed.
    IMPORTANT:
    • If you remove a device from the project that has applications or groups configured, scanning the network will automatically recreate those applications or groups with default names.

    • Do not close the network or project while scanning is in progress.

    • If you try to scan the network device in C-Bus Commission while a network scan is already in progress in the Toolkit, an Error pop-up will be displayed.

  2. Once the scanning is completed, firmware update icon is displayed for the C-Bus Devices, indicating a new firmware is available for the C-Bus Device.
  3. Click to perform firmware upgrade for a respective C-Bus Device.

    Once the firmware is successfully upgraded, re-scanning the Network Devices will display the new firmware version.

    NOTE: After you update the firmware for a selected device and re-scan the Network Device, the firmware icon will no longer be displayed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.