Software Version 2.14.0

Unravel

Unravelling unit address is the process of giving unique unit address to all units within a C-Bus Network.

Unravelling unit address is important when you are adding C-Bus units to the physical address. When new C-Bus units are added to the network which have been previously used on another network, they may be configured with unit addresses that are already taken on the C-Bus Network.

C-Bus network scanning process identifies the C-Bus units with duplicate addresses, which is highlighted as duplicate.

On identifying duplicate the confirmation box is displayed to resolve the conflict.

  1. Select No, to retain the duplicate address.

  2. Select Yes, Confirmation dialog box is displayed to unravel duplicate network devices.

    1. If you select No, the duplicate address is retained.

      This can be resolved manually :

      To unravel duplicate unit addresses, select the device and click select Unravel.

      TIP: Unravel can also be done by right-click Network Devices > Unravel.
    2. If you select Yes, unravelling process is initiated.

    3. Once unravel is completed, the details of unravelled devices and their new addresses are displayed.

      The details can be copied to the notepad for future use or/and close the window.

All the addresses in the network are unique.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.