Software Version 2.14.0

Sort Device

Prerequisites: The devices must already be opened and scanned in a Network.

  1. Click to sort the devices in the live network.

  2. Select Sort from the available options and then select an appropriate sort method.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.