Software Version 2.14.0

Extract All and Deploy All C- Bus Devices

With C-Bus Commission, you can extract and deploy all C-Bus devices between your project and the live network without switching to Toolkit. So, the need to toggle between client applications is minimized, software inefficiencies are reduced and the user experience is enhanced.

When you perform the Extract All/Deploy All function, it extracts/deploys both supported and unsupported devices (in the PROPERTIES window). This includes most of the wired C-Bus device family and also includes the standard Deploy and Extract buttons when selecting a single device or multiple devices.


Prerequisites:

  • The network must be already created.

  • The C-Bus network must be opened, and C-Bus devices must be scanned.

  • Devices for deployment/extraction must be either partially matched or fully matched.


A device is said to be partially matched if the field information of address, unit type and firmware in Devices in Project are same as in Network Devices.

  • If a device is fully matched, then the device can be extracted to the project or deployed to network directly.

  • The below video demonstrates how to extract single device from Network to Project.

To Extract All Devices

  1. In the Network section, click  drop-down and choose Extract — Extract All to Project.

    NOTE: Multiple devices can be extracted only if all of them are fully matched.
    TIP:
    • If a device does not exist in the project, you can add the device in the Project from the library and extract all the live data into the project device.

    • The firmware version of the device added to the project must match the firmware version of the live network device.

    • If a device is partially matched then, the device must be matched fully with the project device in Project. The video of fully matching the devices is demonstrated below:

      Once extract all function is completed, all newly extracted devices are placed with their live network configurations into the project.

To Deploy Single Device/All Devices

  1. Select the device in Devices in Project section and click to deploy selected device to C-Bus Network.

    NOTE: You can select one or more devices.

    The project device information is transferred to the network devices. You can view the Active and Completed status in DEPLOYMENT QUEUE window.

    Active Completed
  2. To deploy all devices to C-Bus Network, click  drop-down and choose Deploy – Deploy All to Network.

    You can view the Active and Completed status in DEPLOYMENT QUEUE window.

    Active Completed
    NOTE: The Deploy - Deploy All To Network will be enabled only when at least one device is in a matched or partially matched state.

    Once deploy all function is completed, all newly deployed devices are placed with their project configurations into the live network.

    The deploy all function will deploy the project device information to the device(s) on the network, regardless of whether the device can be edited in the Property Editor of C-Bus Commission or was previously edited in Toolkit.


    The below table lists the legacy devices supported in C-Bus Commission.

    KEY1

    KEYAUX4

    KEYAV4

    KEYP2

    KEYDV2

    RELDN8SP

    DIMDN4

    PC_INT_1

    PC_PGA

    PC_CTD

    KEY2

    DINAUX4

    KEYA6

    KEYP4

    KEYDV3

    RELDN8B

    DIMDN4F

    PCINT4

    PC_PACA

    PC_CTDL

    KEY4

    KEYBC2

    KEYA8

    KEYP6

    KEYDV4

    RELDC4

    DIMDN8F

    PC_CNIEI

    PCINTU

    PC_WHAM

    KEYIR1

    KEYBC4

    KEYB2

    KEYBIR2

    CLK2

    RELDB1

    DMXDO12

    PC_CNIED

    PCLOCALU

    INT_CIS

    KEYIR4

    KEYM2

    KEYB4

    KEYBIR4

    RELAY1

    RELMB8

    DIMDN8

    PC_CNICI

    EN_UNIV

    INT_AXEZ

    KEYC1

    KEYM4

    KEYB6

    KEYBIR6

    RELAY2

    DSIMB8

    DIMDS8

    PC_CNICD

    PC_MIND2

    EN_AXEZ

    KEYC2

    KEYM8

    KEYH1

    KEYV1

    RELAY4

    ANOMB8

    ANODN4

    PCLOCAL4

    PC_CTB

    INT_CMFT

    KEYC4

    KEYA1

    KEYH2

    KEYV2

    DIMMER4

    DIMPR1

    PC_LOCAL

    PC_CBTI

    PC_CTBL

    EN_CMFT

    KEYCIR1

    KEYAV2

    KEYH3

    KEYV3

    AN_OUT4

    DIMPR2

    PC_INT

    PC_CTA

    PC_CTC

    INT_MIND

    KEYCIR4

    KEYA3

    KEYH4

    KEYDV1

    RELDN8

    DIMPR4

    PC_INT1

    PC_IRT2

    PC_CTC3

    INT_HS

    INT_D16

    INT_ELK

    INT_VIEO

    INT_HUIO

    INT_AQUA

    BRIDGE1N

    BRIDGE1F

    BRIDGE2N

    BRIDGE2F

    GATEWLSN

    GATEWLSF

    RELSM8

    PC_CNICW

    PC_CNIC

    PC_CNIE

    PC_CNIEW

    SYSWSR2

         
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.