Software Version 2.14.0

Open C-Bus Network

Prerequisites: The C-Bus Interface must be connected to the C-Bus Network and the software must be able to communicate to this interface.

The Open Network option opens a network connection to the C-Bus Commission.

To open the C-Bus Network:

  1. Select the network from the project.

    NOTE: When the network is closed, the network appears as shown below:
  2. Click C-Bus Devices.

    In the Workspace window, the Network Devices section appears as shown below before opening the network.

  3. Click in Network Devices section.

    The network opens.

    IMPORTANT: Do not close the network while deployment activities are in progress.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.