Creating a New Modbus Device Profile
If your Modbus device profile is not included in the preinstalled profiles in the controller, you can define your own custom profile.
Follow these steps:
-
File format: Modbus device profiles are distributed as *.json files. You can create and edit these files using a common text editor (such as Notepad or Notepad++). Remember to save the file with the extension *.json.
-
Profile structure example:
{ "manufacturer": "Schneider Electric", "description": "Example device", "mapping": [ { "name": "Output 1", "bus_datatype": "bool", "type": "coil", "address": 0, "writable": 1 }, { "name": "Input 1", "bus_datatype": "float16", "type": "inputregister", "address": 0, "value_multiplier": 0.001, "units": "V" } ] }-
The
"mapping"table in the *.json file contains information for each Modbus register, coil, input, or output. -
Adjust the mapping settings according to your specific device:
Parameter
Description
Type
Required
Name
Object name, e.g. Output 2
String
Yes
bus_datatype
KNX object data type, key from dt table, e.g. float32
String/Number
Yes
type
Modbus register type, possible values: coil, discreteinput, register, inputregister.
String
Yes
address
Register address (0-based)
Number
Yes
writable
Set to true to enable writing to register if type is either coil or register.
Boolean
No
write_only
Set to true to disable reading coil or register value when "writable" is enabled.
Boolean
No
datatype
Modbus value data type. If set, conversion will be done automatically. Possible values: bool, uint16, int16, float16, uint32, int32, float32, uint64, int64, quad10k, s10k
String
No
value_delta
New value is sent when the difference between previously sent value and current value is larger than delta. Defaults to 0 (send after each read).
Number
No
value_base
Add specified number to the resulting value.
Number
No
value_multiplier
Multiply resulting value by the specified number,value = value_base + value * value_multiplier.
Number
No
value_bitmask
Bit mask to apply, shifting is done automatically based on least significant 1 found in the mask.
Number
No
value_nan
Array of 16-bit integers. If specified and read operation returns the same array no further processing of value is done.
Array
No
value_conv
Apply one of built-in conversion functions
String (Int)
No
value_custom
Name of a built-in enumeration or a list of key -> value mapping, resulting value will be 0 if key is not found.
String/Object
No
internal
Not visible to user when set to true, should be used for scale registers.
Boolean
No
units
KNX object units/suffix
String
No
address_scale
Address of register containing value scale, value = value * 10 ^ scale
Number
No
read_count
Number of register to read at once (for devices that only support reading of a specific block of registers)
Number
No
read_swap
Swap register order during conversion (endianness)
Boolean
No
read_offset
Position of first register of data from the block of registers (0-based).
Number
No
timeout
Specify device timeout in seconds.
If the extension device does not reply within specified time, it is considered as timeout error.
Default values: 0.5 s for Modbus RTU, 3 s for Modbus TCP
Number
No
write_multiple
This parameter set the multiple writing function (function 15 or 16 is used instead of function 5 or 6).
If "Type" is set to "register" and "Write_multiple" is set to "true", Modbus function 16 is used for writing to the register.
If "Type" is set to "coil" and "Write_multiple" is set to "true", Modbus function 15 is used for writing to the coil.
Default value is "false", which means that Modbus function 5 or 6 (depending on register type) is used for writing.
String
No
-
-
Upload to the controller:
-
Once you have created your *.json file with all the necessary profile information, upload it to the controller via Configurator → Modbus → Profiles → Add profile.
-
-
Best practice:
-
When creating a new device profile, consider using an existing profile as an example or template. You can download existing profiles from the controller to understand the structure and syntax.
-
For detailed instructions on custom device profile creation, refer to the application note available at Schneider Electric website.