250929_LSS100100/LSS100200_SW_03.0

Launching PC Visualization

  1. Ensure that your PC or tablet device can access the controller.

  2. Open a web browser and enter the controller IP address (default: 192.168.0.10).

  3. Click on the Start page.

  4. Select the desired plan.

  5. To maximize the map visibility, you can minimize the sidebar by clicking .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?