250929_LSS100100/LSS100200_SW_03.0

Schedulers

Schedulers enable end users to control KNX group address values based on the date or day of the week. Users can add events and enable/disable schedulers as needed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?