250929_LSS100100/LSS100200_SW_03.0

Touch Application

In the Touch application, you can view all the features configured in the Touch Config, including floors, rooms, widgets, and functions.

On the left side of the screen, you’ll find the main menu, which includes:

  • Menu: This can be locked by clicking the menu icon , at which point the icon will rotate vertically.

  • Floors: This displays a list of all floors and rooms.

  • Functions: This section presents groups of widgets, categorized by their respective functions.

At the top right of the screen, you can notice a lock icon . When this icon is unlocked (click it), it enables you to edit individual widgets using the editing pencil. This allows you to change their names, set widget visibility in the mobile application, initiate voice control, and configure schedulers for widgets.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?