250929_LSS100100/LSS100200_SW_03.0

Import KNXPROJ File

You can directly import the *.KNXPROJ file into the controller using the Import KNXPROJ file button.

This process preserves the structure of the project and the data point types (DPTs) of the group addresses, including automatic units and suffixes.

  • File: Choose the file you want to import.

  • Password: For password-protected *.knxproj files, you will need the password set in ETS. Without the correct password, the import process cannot proceed.

  • Add objects without data type: The import process allows you to add objects without defined data types.

  • Add level names to objects: You can assign structure level names to the objects.

  • Import security keys: By default, this option is enabled. When enabled, the backbone key and KNX data secure keys for group objects will be automatically filled in after the import.
    See also Add New Object.

  • Create filtering table from the project data: If you check this option, filtering tables from a KNX project will be automatically created.

  • Set group address filtering policy to “Accept”: When enabled, the DST group policy will automatically accept selected group addresses in:
    ConfiguratorNetworkKNX ConnectionIP > Local Filter (IP > Local Filter) and Local > IP Filter (Local > IP Filter).
    If this option is unchecked, the DST group policy remains unchanged.

NOTE: Objects with the same name are considered duplicates and might not be imported. These objects will be marked as discarded.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.