250929_LSS100100/LSS100200_SW_03.0

Upgrade Firmware

  1. Navigate to SystemUpgrade Firmware to upgrade the system.

    NOTE: The controller firmware downgrade is not recommended.
  2. Choose your firmware and signature files and click OK.

    NOTE: Starting from firmware version 3.0.0, you are required to add a signature file. Without this file, the firmware upgrade will not be performed.

During the firmware upgrade, the device may not respond as the controller undergoes several reboots. The upgrade process can take up to 5 minutes, especially when a significant amount of trend data is used in the project.

While the upgrade is in progress, LED1 will flash red/green. Please ensure that the controller remains powered on until LED1 ceases to flash red/green.

IMPORTANT: After each upgrade, it is strongly recommended to clear your browser cache to ensure optimal performance.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?