250929_LSS100100/LSS100200_SW_03.0

ETS 6

To integrate the controller with KNX TP (Twisted Pair) UART/IP functionality and program it alongside other KNX bus devices, follow these steps:

  1. Add the controller to ETS Connection manager:

    • Open ETS 6 and navigate to Bus > Manage configured connections.

    • If your controller is on the same network as a computer running ETS 6, it can be discovered automatically. If discovered, double-click on the item in the Manage configured connections list to choose it.

    • If not discovered, proceed to the next steps.

  2. Manually configure the interface:

    • On the Manage configured connections tab, click the green “+” icon.

    • Select IP Tunnelling.

    • Click IP Tunnelling (0.0.0.0:3671).

    • In the settings tab on the right-hand side:

      • Set the Name of your connection.

      • Specify the Server (IP address of the controller).

      • Set the Port.

  3. Test communication with ETS:

    • Click Test in the lower-right corner to verify communication between ETS and the controller.

    • If the test is successful, double-click on the item in the list of interfaces to set it as active.

    • The current interface is now set up.

NOTE: Port 3671 is blocked from any public IP address.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?