250929_LSS100100/LSS100200_SW_03.0

ETS 5

To integrate the controller with KNX TP (Twisted Pair) UART/IP functionality and program it alongside other KNX bus devices, follow these steps:

  1. Add the controller to ETS Connection manager:

    • Open ETS 5 and navigate to Bus > Connections > Interfaces.

    • If your controller is on the same network as a computer running ETS5, it can be discovered automatically. If discovered, double-click on the item in the Discovered interfaces list to choose it.

    • If not discovered, proceed to the next steps.

  2. Manually configure the interface:

    • Click the green “+” icon next to the Configured interfaces.

    • Select IP Tunnelling.

    • Click New Connection (0.0.0.0:3671) (which is created in the Configured interfaces).

    • In the settings tab on the right-hand side:

      • Set the Name of your connection.

      • Specify the Server (IP address of the controller).

      • Set the Port.

    • Select the interface you configured in the previous step.

  3. Test communication with ETS:

    • Click Test in the lower-right corner to verify communication between ETS and the controller.

    • If the test is successful, double-click on the item in the list of Configured interfaces to set it as active.

    • The current interface is now set up.

NOTE: Port 3671 is blocked from any public IP address.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?