250929_LSS100100/LSS100200_SW_03.0

Adding a New Modbus Device

To add a new Modbus device to your controller configuration, follow these steps:

  1. Click the Add device button in the Modbus tab.

  2. Configure the parameters in the Modbus device dialog as follows:

    • Connection type:

      • Choose either RTU (RS-485) or TCP/IP as the connection type for your Modbus device.

    • Name:

      • Define a name for the Modbus device.

    • Status object:

      • Monitor the connection status with the Modbus device using the Status object.

      • When communication is disrupted, the status object is set to 0.

    • Write to bus:

      • Enable sending data to the KNX TP bus.

      • If disabled, telegrams to KNX TP are not sent when the Modbus value changes. Telegrams are still sent to KNX IP.

    • Profile:

      • Select the Modbus profile for your device.

      • You can use a preinstalled profile or upload a custom device profile to the controller.

      • Refer to the procedure for creating a new profile definition (Creating a New Modbus Device Profile).

    • Device address:

      • Set the extension address of your Modbus device.

    • Poll interval (seconds):

      • Specify how often values are polled from the Modbus extension device.

      • A value of 5 means new values are read every 5 seconds.

    • Timeout (seconds):

      • If there is an error in the connection, the device will wait for the specified time and then send an error message to the Error log.

    • IP (Modbus TCP):

      • If you are using Modbus TCP, set the IP address of the Modbus device.

      • If the Modbus device is connected via a Modbus gateway, set the gateway IP address here.

    • Port (Modbus TCP):

      • Set the port for Modbus TCP communication.

      • The default value according to the Modbus standard is 502.

    • Persistent connection:

      • When enabled, the connection remains open.

      • When disabled, the controller reads all registers and disconnects.

    IMPORTANT: Some Modbus TCP/IP devices may not handle frequent (re)connections well (e.g., panel servers, inverters, Modbus meters). Consider using the Persistent connection option if your polling interval is less than a minute.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.