KNX → EnOcean Mapping
In the Configurator section under EnOcean → EnOcean >> KNX, you can enable the capability to control EnOcean devices (such as actuators and dimmers) from your KNX installation via the controller.
Here’s how it works:
-
Device simulation:
-
The controller simulates the behavior of specific EnOcean devices.
-
For example, an EnOcean switch actuator can be controlled by an EnOcean rocker switch.
-
To achieve this, the controller emulates the function of the rocker switch and manages the switch actuator.
-
-
Configuration steps:
-
Start by defining the device to be simulated by the controller.
-
Click the Add new device button in the lower-left corner.
-
In the Device dialog, specify a unique Address, Device name, and Profile. The profile represents the function of the device simulated by the controller.
-
Click Save.
-
-
Pairing with EnOcean devices:
-
Mapping to KNX Addresses:
-
The device created in the controller can now be mapped to specific KNX addresses.
-
Click
on the desired line in the device list to open the Device
mapping dialog. -
Select the appropriate controller object from the drop-down menu or create a new object directly from the dialog using the
icon. -
Make sure to tick the Send telegram option. Otherwise, the EnOcean telegram will not be transmitted.
-
Click Save.
-
When the KNX object value changes, a telegram is sent to the device paired with the controller virtual device.
-