250929_LSS100100/LSS100200_SW_03.0

Import Neighbours

This feature allows you to import objects that have been marked for export from another Wiser for KNX/SpaceLYnk.

The system will prompt you for the remote password of the second device from which data will be exported.

To access remotely, modify the IP and password according to your controller settings. For example: https://remote:remote@192.168.0.10/scada-remote?m=rss&r=alerts

NOTE: The export option must be activated for objects in order to share them between Wiser for KNX/spaceLYnk. Enabling this option makes objects visible via BACnet and remote services (XML/JSON).

Single Wiser for KNX/spaceLYnk in IP network

Multiple Wiser for KNX/spaceLYnk controllers

NOTE: Remote services must be enabled on both devices for object sharing: SystemServicesRemote servicesService status: Enabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?