250929_LSS100100/LSS100200_SW_03.0

Supported BACnet Interoperability Building Blocks (BIBB)

Data Sharing

ReadProperty-B

DS-RP-B

ReadPropertyMultiple-B

DS-RPM-B

WriteProperty-B

DS-WP-B

COV-B

DS-COV-B

Device and Network Management

Dynamic Device Binding-B

DM-DDB-B

Dynamic Object Binding-B

DM-DOB-B

DeviceCommunicationsControl-B

DM-DCC-B

TimeSynchronization-B

DM-TS-B

UTCTimeSynchronization-B

DM-UTC-B

ReinitializeDevice-B

DM-RD-B

BACnet Object Types Supported

  • Device

  • Analog Value

  • Binary Value

Data Link Layer Options

  • Media: BACnet IP

  • Option: Register as a Foreign Device

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?