250929_LSS100100/LSS100200_SW_03.0

Text Label

Text labels can be added and moved across the visualization map. Configure the parameters for your text label in the Text label tab as follows:

  1. Text:

    • Enter the label text.

  2. Font size:

    • Specify the font size for the label.

  3. Text style:

    • Choose the style for the text (bold, italic, underscored).

  4. Custom font:

    • Provide the font name (if applicable).

  5. Font color:

    • Set the label font color.

  6. Additional classes:

    • Creates custom CSS classes to modify graphical objects.

Once the label parameters are defined, click the Add to plan button, and the newly created label will appear on the map.

You can move the label to your desired location.

Remember to adjust the element size and position (refer to Object).

Finally, click Save and reload plan to activate the label.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?