250929_LSS100100/LSS100200_SW_03.0

KNX Specific Configuration

To configure KNX connection, follow these steps:

  1. Navigate to Configurator > Utilities > System > Network > KNX connection for detailed configuration options.

  2. After making changes, look for the Apply changes icon in the top-right corner and click it.

  3. The controller  will automatically reboot after changes are applied.

NOTE: Starting from firmware version 2.6.1, the controller now supports KNX long frames with a maximum length of 55 bytes. This improvement significantly reduces the download time required for commissioning KNX devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.