250929_LSS100100/LSS100200_SW_03.0

Touch Visualization

The Touch Visualization offers a streamlined and visually appealing way to create automation interfaces:

  1. Ease of use:

    • Setting up the Touch visualization is straightforward.

    • You will spend significantly less time compared to visualization as described in Visualization.

  2. Perfect for touch screens:

    • Designed with touch screens in mind, it provides an intuitive user experience.

    • Interact effortlessly with your smart home or building automation system.

  3. Pre-made widgets:

    • The included widgets cover essential automation functions.

    • Quickly build your interface without starting from scratch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?