250929_LSS100100/LSS100200_SW_03.0

Scheduler → Holidays

When an event is scheduled to run on a holiday (Scheduler → Events), the Holidays button for holiday entries will be activated in the Schedulers tab. To set up holidays, follow these steps:

  1. Click the Holidays button.

  2. Click Add holiday.

  3. Fill in the Holiday dialog as follows:

    • Name: The name of the holiday.

    • Holiday type: Select either a specific date or a day of the week.

    • Day: The day on which the holiday will be active.

    • Month: Specify the month during which the holiday will be active.

    • Year: Leave this blank for recurring events.

    • Duration (days): Set the duration of the holiday.

  4. Click Save.

Your holiday will appear in the list of holidays.


NOTE: Using the Scheduler visualization on a smartphone is not recommended.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?