250929_LSS100100/LSS100200_SW_03.0

Profiles

All uploaded Modbus profiles are displayed in a table that appears when you click the Profiles button in the Modbus tab. Here’s what you can do with these profiles:

  1. Delete profiles:

    • Click associated with each profile to delete it.

  2. Download profiles:

    • Click to save a profile as a .json file.

    • You can then use this downloaded profile for further customization.

  3. Modify profiles:

    • If you need to read/write registers not available in the preinstalled profile, consider modifying it according to your specific requirements.

    • Upload the modified profile back to the controller the Add profile button at the bottom left of the Profiles table.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?