250929_LSS100100/LSS100200_SW_03.0

Routes

A routing table is a data structure that itemizes the paths to various network destinations. It encapsulates details about the immediate network topology.

The system routing table can be found under the SystemNetworkRoutes.

The window is divided into two sections:

  • Dynamic routes

  • Static routes

Dynamic routes

This section displays a list of network destinations that the system has learned on its own, along with the automatic selection of the ‘optimal route’.

It includes:

  • Interface: This is the name of the local interface responsible for reaching the gateway.

  • Destination: This is the IP address of the destination subnet, which, in conjunction with the network mask, defines the network ID.

  • Gateway: This is the IP address of the gateway through which the network can be accessed.

  • Network mask: This shows the network mask address.

Static routes

These are routes manually entered into the controller routing table. They do not change automatically.

It includes:

  • Interface: This is the name of the interface.

  • Destination: This is the IP address of the destination.

  • Gateway: This is the IP address of the gateway.

  • Network mask: This is the network mask address.

  • Flags: These are useful for troubleshooting network issues.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?