250929_LSS100100/LSS100200_SW_03.0

Restore

The restore function allows you to reinstate the configuration from a backup file.

To restore the system, follow these steps:

  1. In the Utilities tab, click the Restore button.

  2. Select the Choose File option and locate your backup file.

  3. After selecting the file, click the Save button to initiate the restore process.


The maximum backup size is 32 MB. Projects larger than this cannot be restored.

When creating a backup, you will be prompted to choose a password. This password will be required when you wish to restore the project from the backup file.

During the restore process, if LED 1 is flashing red/green, it indicates that data are being recalculated. It is important not to switch off the controller until the process is complete. This ensures the integrity of the restored data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?