250929_LSS100100/LSS100200_SW_03.0

Widgets

A widget is a small web page that can be attached to a button and pops up when activated.

To add a widget, follow these steps:

  1. Click next to the Widgets folder → select Add.

  2. Or click the Add new widget button.

  3. Fill in the Widget dialog.

NOTE: The content of the widget should be defined under the Visualization tab. Additionally, ensure that the widget size is smaller than the plan on which it is placed.

Your new widget will appear in the Layouts/Widgets tab. You can further edit it, duplicate it along with all its components, export or delete it.

An empty widget (with no objects) will not be visible in the visualization.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?