250929_LSS100100/LSS100200_SW_03.0

Touch Config Menu

When you click in the top right corner of the screen, the Touch Config menu opens with the following options:

  1. Backup config: Allows you to back up the Touch visualization settings.

  2. Restore backup: Enables you to restore previous Touch visualization configurations.

  3. Settings: Access general settings for the Touch.

  4. Styles: Manage general styles for visualization and widgets.

  5. Clear all: Clears settings for rooms, widgets, and styles.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?